A carnival scam: The secret behind the "Ladder Climb Carnival Game"

Fun
Why is the ladder climbing carnival game so hard to beat? It's not because of you, it's because of a scientific cheat!
Uploaded from script

We've all been duped by these games at amusement parks and on seaside bridges. The bottlering toss, the baseball bottle toss, the basketball three-point shots. Why are these games, which seem so easy at first glance, so difficult? It's not you. It's the science.

 

The showmen intentionally make these games look easy on the outside to lure you in, but behind the scenes they've built in clever physics that make winning much more difficult, almost impossible.

 

One example of this is climbing the ladder. At first glance, it seems simple: climb the hanging ladder on all fours to the top and win a giant cuddly toy. But there's a reason why the prizes in this game are so big. It's very hard to win...

 

Former NASA and Apple engineer Mark Rober explains in his video "Carnival Scam Science (and how to WIN)" the basic physics that make this game so difficult, and the secret to beating it.

 

Unlike a rope bridge, which is supported by two points at each end, the carnival ladder is supported by one point at each end. This is important because it derails your body's aid in keeping you balanced: Your center of mass.

 

The center of mass is the point on an object where all the weight is evenly distributed. If you are trying to balance something on your finger, the point on the object where it can balance itself without outside help is its center of mass. To keep the object balanced, you must keep the center of gravity within the support area:

 

Hand balancing soccer ball on single finger, with center of mass marked. Engineering a Carnival Scam: The Secret Behind the Carnival Ladder Climb

 

When standing, a person's center of support is between the heels and the tips of the toes. To keep your balance when standing, you must keep your center of gravity between these two points:

 

side view of person with center of mass and area of support marked. Engineering a Carnival Scam: The Secret Behind the Carnival Ladder Climb

 

Therefore, when you bend down to pick up an object from the floor, you automatically stick your butt out; your body naturally keeps your center of gravity between the two points of support so you don't fall over.

 

When you crawl over a conventional rope bridge, the support area is located between all four end points of the bridge, i.e. over a fairly large area. Since the carnival ladder only has one point at each end, the support area is just a line. You are basically crawling across a wire rope:

 

person crawling across a rope bridge connected with four points total, area of support marked. Engineering a Carnival Scam: The Secret Behind the Carnival Ladder Climb

 

This may look similar to a slackline, but a slackline is easier because you can move your arms and legs to keep your center of gravity above the support line.

 

The secret to beating the carnival rope ladder? Keeping your center of gravity above a line, which unfortunately you can only do well with a lot of practice.

 

person crawling across a rope bridge connected with two points total, area of support marked. Engineering a Carnival Scam: The Secret Behind the Carnival Ladder Climb

 

Our advice: stop climbing the ladder and ride the rollercoaster instead!

 

Just as carnival games challenge your understanding of physics, finding the right components for your engineering projects can feel like a tricky puzzle. But with 3Dfindit, you can streamline your design process by quickly finding the exact CAD, CAE and BIM models you need from a massive library of over 6,000 catalogs. No more walking like you're balancing on a tightrope - with 3Dfindit, finding the right parts is as easy as riding a roller coaster. Start designing your next big project today!

 

3Dfindit lets you construct new and wild things! Download 3D CAD, CAE and BIM maker models in over 100 different formats from over 6,000 catalogs NOW!